Profinet View & DCP (requires Npcap or Winpcap):
- Scans and displays all DCP-enabled devices on the network
 
- Identifies specific information about connected Profinet devices
 
- Performs specific device actions:
- Customizes IP Address, Profinet Device Name, Subnet Mask, Gateway
 
- Different Reset Modes 
 
- Wink for visual identification
 
 
 
Diagnose View:
- Scans the Turck devices on the network and flags devices with existing diagnostics
 
- Displays the device status or diagnostic message
 
- Direct link to the creation of the diagnostic report 
 
- Accessing the detailed diagnostics page of the affected device
 
 
Monitoring and visualization of EZ-Array light curtain with light beams that can be switched on and off.
 
Optional: start of a DHCP server with the following functions
- DHCP Scan List
 
- DHCP Start/Stop
 
- DHCP Get Adapter List
 
 
Visualizes the time sequence of process input data of connected analog devices/sensors
 
CODESYS recipes  and/or log files (USB data) are uploaded to the PC