EDS for Turck Ethernet/IP gateways


Major version 2:  Two variants of the EDS for this product are supplied:


Standard file, e.g. BL67-GW-EN-IP_R2.eds
	This one allows uploading from and downloading to the device in Omron Network Configurator. 
	Configuration is possible only after uploading the valid data sizes from the device
	(because the data sizes are may not be edited).


RW_ file, e.g. RW_BL67-GW-EN-IP_R2.eds
	This one (RW_) allows editing the data sizes, enabling offline configuration. 
	Upload from the device is possible, but download to the device is not.
	
	
Note: 
Only the files for BL67-GW-EN (Multiprotocol) support configuration with RSLogix V20. 
All other files don't support this yet.

The BL67-GW-EN-4F uses the same EDS like the BL67-GW-EN as only the power Connector is different.

The BL67-PG-EN-V3 as CODESYS Programmable device uses the Turck CDS3.eds.