Catalog files for Turck BL67-GW-EN 'multi protocol' gateways.

These files may be importet by Rockwell RSLogix5000, in order to configure these Turck devices in 'CIP bridging mode'.
See user documentation for details!


------------------------------------------------------------------------------------------------------------------------

Two variants of the catalog file are supplied:

xxx_CLX_V19_xxx.L5K
		Created by RSlogix5000 revision 19.
		Cannot be opened with prior revision (an error message would appear).
		This file may not be used with RSLogix Mini or Lite Edition.

xxx_CLX_LITE_V20_xxx.L5K
		Created by RSlogix5000 revision 20.
		Cannot be opened with prior revision (an error message would appear).
		This file is designed for RSLogix Mini or Lite Edition.


Note:
The BL67-GW-EN-4F uses the same EDS like the BL67-GW-EN as only the power Connector is different.