Hans Turck GmbH & Co KG - Witzlebenstr. 7- 45472 Mülheim an der Ruhr - Germany - Sensoren - Interface - Feldbus - Sensoren - Interface - Feldbus - Sensors - Interfaces - Fieldbuses - Sensoren - Interface - Feldbus - Sensors - Interfaces - Fieldbuses
  Home  Sitemap  About us  Contact  Products  Support  News  
  news  Infoarchive  Fairs  
- Sensoren - Interface - Feldbus - Sensors - Interfaces - Fieldbuses

  BL67 - Outgrowing the Switching Cabinet
In a distributed installation of machines and systems, the I/O signals have to be processed directly in the field. An efficient solution in this context is a modular I/O system with protection rating IP67

BL67 - I/O Device
One of the present trends in automation is the distributed, remote installation of machines and systems with the help of modular peripheral devices. This is particularly reflected by the development of the fieldbus market, where PROFIBUS is on constant course for growth. From 2004 until the end of 2007, the Profibus User Organisation has planned to double the number of installations from 10 to 20 million stations.
In 2004, more than 2.5 million new stations were installed, so that the manufacturers of Profibus devices could benefit from an annual turnover increase of 30% per cent; for 2005 the PNO is expecting further growth.

Fieldbus technology is largely concerned with remote peripheral devices, but which requirements must these meet in more concrete terms? I/O systems for the IP20 area, mounted in a protective control cabinet, are part of the well-established technology in this field. This first idea that springs to mind is to simply install these IP20 systems in a separate protective housing and to mount this directly at the machine base. This concept would surely shorten the cable routes to the peripheral sensors, but has no other distinct advantages. The user would still have to invest a lot of time to route the sensor cables, lead these through cable glands and wire them to the IP20 bus terminals. Polarity errors, which negatively affect valuable installation and set-up times, can easily occur. And if the fieldbus station is to be expanded by some other signals, then problems are bound to occur. Additional cable glands have to be integrated into the protective housing, which, at worst, may not provide enough space for such additions. And this is exactly where IP67 fieldbus devices come into play. Their percentage share within the fieldbus market is growing continuously. According to estimations, the number of fieldbus stations, which may be mounted directly in the field due to their high protecting rating, will account for 15% of the fieldbus turnover in 2005...

The author
Markus Ingenerf
is product specialist for BL67
within the product marketing
team of TURCK Headquarters

Download full size editorial:

 Proceed directly to product database.
BL67 - Outgrowing the Switching Cabinet >>>download<<<

<<< back

 Address

Turck Australia Pty Ltd
Unit 5,6-7 Gilda Court
Mulgrave, 3170. Victoria
Phone:1300 132 566
Fax: 03 9560 1620

PO Box 5037 
Brandon Park, Victoria. 3150


  more@TURCK


Customer magazine

 TURCK Worldwide