Hans Turck GmbH & Co KG - Witzlebenstr. 7- 45472 Mülheim an der Ruhr - Germany - Sensoren - Interface - Feldbus - Sensoren - Interface - Feldbus - Sensors - Interfaces - Fieldbuses - Sensoren - Interface - Feldbus - Sensors - Interfaces - Fieldbuses
  Home  Sitemap  About us  Contact  Products  Support  News  
  news  Infoarchive  Fairs  
- Sensoren - Interface - Feldbus - Sensors - Interfaces - Fieldbuses

News
 Newest applications and product informations...

 Interface technology: Knowing Where's the Fault
Intelligent interface devices diagnose the route between the field device and the control system. Whenever the subject of diagnostics is discussed today, people usually think of the associated functions in control systems or field devices.

 Pressure and temperature sensors
Pressure and temperature are frequently used measuring variables, for which great importance is placed on the interfaces to the process and the operator, as well as accuracy and reproducibility.

 Magnetic Field Sensor for Pneumatic Cylinders Ensures Reliable Monitoring
Magnetic field sensors for monitoring the position of pistons in pneumatic cylinders are standard in industrial automation.

Further information can be found in our INFOARCHIVE >>>

 Address

Turck Australia Pty Ltd
Unit 5,6-7 Gilda Court
Mulgrave, 3170. Victoria
Phone:1300 132 566
Fax: 03 9560 1620


  more@TURCK


Customer magazine

 TURCK Worldwide